Browse FAQs

How to setup a Tesys LTMR to talk to a Magelis over E/IP?

Published date: 16 January 2019

Issue: Looking for a guide that describes how to setup a Tesys LTMR to talk to a Magelis over E/IP.

Product Line: Magelis (XBTGT, XBTGH, XBTGK, HMIGTO, HMIGTU, HMISTO, HMISTU),  Tesys LTMR, Vijeo Designer

Resolution: Attached is a guide on how to setup the LTMR to talk to an Allen Bradley PLC over Ethernet/IP. These are the same steps taken when setting up the LTMR to talk to a Magelis. Once the LTMR is setup, you would need to use the Generic Ethernet/IP (explicit) driver in Vijeo Designer.  This driver can be found under the Generic Drivers Manufacturer in the New Driver dialog. From there, you would need to setup some variables in Vijeo Designer to get/set the parameters from the LTMR. Be sure to use the "Vendor Defined" class and set the instance according to the instances available on the LTMR.On pg 22 and forward of the PDF, there are some instances listed

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.