Browse FAQs

What are the replacement bulbs for the 9001 Type O pilot lights?

Published date: 16 January 2019

Issue:
Looking for the replacement bulb only for the 9001OR120. 

Product Line:
9001 Type O.  9001O pilot light, instrument type

Environment:
all

Cause:
Replacement parts

Resolution:
The 9001 Type O pilot lights used an incandescent bulb.  The bulbs are available in 12V, 24V and 120V.  Since the bulbs are incandescent, the color of the lens does not matter.  An LED replacement bulb is not offered. 

12V - part number 25501-05003 (obsolete).  Sylvania bulb number is 12PSB
24V - part number 25501-05004.  Sylvania bulb number is 24PSB
120V - part number 25501-05005.  Sylvania bulb number is 120PSB

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.