Browse FAQs

Can not download and transfer button grayed out even if licensed with Vijeo XD 3.0

Published date: 16 January 2019

This is du to trial licenses installed on the PC.
To solve the issue you have to delete all the two Trial Licenses listed
The last full license installed and registered will provide the good the required behaviour.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.