Browse FAQs

On an ATV660, Is it possible to disable bypass?

Published date: 20 March 2019

Issue:
 Customer wants to disable the bypass

Product Line:
ATV660

Environment:
Enclosed product

Cause:
n/a

Resolution:
ATV660 was ordered with Bypass but can't use Bypass without blowing out duct work. With the TeSys Overload, there is a contact used to pull in the BC, see schematic, remove wire from that contact and wire-nut for safety.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.