Browse FAQs

Can I use SoMove with the ATV212 drive?

Published date: 06 March 2019

Issue:
Can I use SoMove with the ATV212 drive?

Product Line:
Altivar 212

Environment:
All serial numbers

Cause:
Customer wanted to use SoMove to program ATV212, but the ATV212 was not listed in the SoMove device options.

Resolution:
SoMove will work with the ATV212 drive if the firmware is V5.1 or higher.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.