Browse FAQs

Can't install UPV13.1 after uninstalling EcoStruxure™ Control Expert V14.0

Published date: 20 December 2018

When Installing UP13.1 after uninstalling EcoStruxure Control Expert V14.0, The following error message came up and preventing to complete the installation 
Error during the initialization of the programming unit (initialization of the STMSDK COM object): Unexpected exception (memory allocation, ...)
 After uninstallation of EcoStruxure Control Expert V14.0 and before reinstallation of UPV13.1 do the following
 remove the files in C:\Program Files (x86)\Common Files\Schneider Electric Shared\RAT

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.