Browse FAQs

Do I need to register a licence for using the Software ZelioSoft

Published date: 20 December 2018

Zeliosoft is a software free downloadable from Schneider website
With any software version below to V5.0, there is no software registration or licensing

ZelioSoft version V5.1 and above an brings an optionnal Registration (one licensing)  .  It means the software is working correctly with all features also if no registration is done
There is no need to have the  Schneider Electric Licence Manager already installed into the computer to install or use ZelioSoft V5.1


For Zeliosoft5.1 the registration had been defined as follows:
-Zeliosoft is using a non-copy-protected license
-Zeliosoft does not come with a local trial license
 
We have 2 different way to register:

   
Into the welcome screen “Register Now”


or 

    Into the Menu “File”


The licensing require to have a Web user Schneider account ( this account is used for any Schneider software
)

Once registration is done, news and version update information are automatically provided


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.