Browse FAQs

Why am I unable to change the Dual Rating on the Altivar Process drives?

Published date: 18 December 2018

 Issue:
Trying to change the Dual Rating from Normal Duty to Heavy Duty but getting an error message "DRT no information available"

Product line:
Altivar Process, ATV630

Environment:
n/a

Cause:
n/a

Resolution:
The message "DRT no information available" is not an error message.  According to Level 3 support, this should only show on the display if the customer uses the Info button while looking at the Dual rating parameter.  If the customer is still unable to change the Dual Rating from the keypad, they can try to upgrade the firmware to the latest revision available.  Or use SoMove to access the parameter and change it from Normal to Heavy Duty.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.