Browse FAQs

What are the dimensions for the Altivar Process drives when using the Flange kits?

Published date: 18 December 2018

 Issue:
Looking for the dimensions of the drive inside the cabinet when mounting with the flange kits

Product line:
Altivar Process, ATV630, Altivar 600

Environment:
n/a

Cause:
Replacing ATV61 or ATV71 with flange kit inside enclosed drive package.

Resolution:
The most recent installation bulletin, EAV9843101 for the flange kit shows the dimensions on page 4.  See attached.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.