Browse FAQs

How do I extract a bit of a word In Vijeo Designer with the EIP Driver?

Published date: 18 December 2018

Issue:
How to extract a bit of a word in Vijeo Designer when linking the tags to the Ethernet IP native driver

Environment:
Vijeo Designer 

Resolution:
The Ethernet IP Native driver is tag based.

When linking the tags to the l5k file, the address will be something like this MyArray[0] for an array variable.
To read bit 0 of the first element of the array, you can create a new external bool and enter this address syntax ARRAY[0].0 
It is important to note that is it case sensitive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.