Browse FAQs

What register can I read to determine if my LTME is in Local or Remote mode?

Published date: 17 December 2018

Issue:
Need to be able to determine if Tesys T product is in local or remote mode by reading an internal communication register.

Product Line:
Tesys T LTMR 

Environment:
All models, All serial numbers

Cause:
Information difficult to locate.

Resolution:
Bit 14 of logic register 455 (Canopen index 2004 : 06, Devicenet path 68 : 01 : 06) can be used to determine local/remote mode.   If bit 14 is high then the Tesys is in local mode, Low = Remote mode

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.