Browse FAQs

Preventa XU - TUV certificate of the XUSL4MA and XUSL4MB, type 4 light curtains with built-in muting function

Published date: 21 December 2018

Find attached the TUV certificate of the XUSL4MA and XUSL4MB, type 4 light curtains with built-in muting function, valid up to december 2022

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.