Browse FAQs

What would cause the ATV58 drives to be stuck in the rdy mode and not run?

Published date: 13 December 2018

Issue:
ATV58 drive is stuck in the rdy 

Product Line:
Flex58, ATV58, TRX 

Environment:
All 

Cause:
Drive not getting a run command. 

Resolution:
No 24vdc  voltage on LI1 for the run command
also check the speed reference to make sure the reference is above 0 hz. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.