Browse FAQs

How is the data retained on the XBTGT2930?

Published date: 26 July 2019

Issue:
Looking for an explaination or description of where and how the system settings are retained on a Magelis XBTGT2930.

Product Range:
Magelis XBTGT2930 series

Resolution:
The Magelis XBTGT2930 series contains a lithium-ion battery used for 512K SRAM backup. This will save all system settings such as clock, date, IP address. It is also used for application storgage for Alarms, Data Logging, Event logging, and Retentive Variables.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.