Browse FAQs

Can I control Output 1 and output 2 (terinals 13-14 and 23-24) independently via Profibus on my LTMR Tesys T motor controller?

Published date: 12 December 2018

Issue:
I need to control output 1 and output 2 of my LTMR Tesys T product indpendent of each other, via Profibus network control.

Product Line:
LTMR Tesys T product 

Environment:
Models containing Profibus network 

Cause:
Unable to find answer in current literature.

Resolution:
It is not possible to control output 1 and 2 independent of each other via Profibus.  These output behave as a single output and both change state at the same time.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.