Browse FAQs

Osisense XC - What is the difference between both limit switches XCKN2118G11 and XCKN2118G11TQ?

Published date: 12 December 2018

The XCKN2118G11 is a basic limit switch already sold in a collective package of 20 units. The "XCKN2118G11TQ" reference does not exist in standard basic limit switches shown in the Osisense XC standard catalogue (https://download.schneider-electric.com/files?p_Doc_Ref=DIA4ED2170406EN). For some limit switch references, "TQ" suffix means collective package of XX units. Attached the packaging label of the XCKN2118G11 standard part number, showing the unit quantity delivered. In XCKN series, some TQ references exist in adapted products with quantity different from 20; examples XCKN2118P20TQ containing 60 units or XCKN2110G11TQ containing 40 units

Was this helpful?

What can we do to improve the information ?