Technical FAQs

Ask a Question

Can we use the Omron CS1W-EIP21 module to communicate over FINS Ethernet on the Magelis HMI?

Issue: The documentation of Vijeo Designer does not show the CS1W-EIP21 as a supported communication module for the Sysmac FINS Ethernet driver.
 
Product Range: XBTGT, XBTGK, XBTGH, HMISTO, HMISTU, HMIGTU, iPC

Resolution: According to the specs of the Omron CS1W-EIP21 module, it supports the Sysmac FINS commands in addtion to the E/IP commands. Therefore, the Magelis HMI will be able to communicate to the Omron PLC via this module using the Sysmac FINS Ethernet driver in Vijeo Designer.
Was this helpful?
What can we do to improve the information ?