Browse FAQs

Preventa XU - What is the first-up time of the XUSL4MA or XUSL4MB light curtains with integrated muting

Published date: 21 December 2018

Definition of the first-up time (or TON): After a power-up, the system is performing self-tests for checking its integrity. The first-up time is the delay, from power-up, after which the system is ready for operation. The first-up time of the XUSL4MA & XUSL4MB light curtains with integrated muting is lower than 10 second (10s)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.