Browse FAQs

Osisense XC - Can I replace the ZCKJ404 switch by the ZCKJ4 body+ZCKE05 head?

Published date: 07 December 2018

Even if both switches have a 2-step special contacts, ZCKJ404 or ZCKJ404H29 or ZCKJ404* switch cannot be replaced by ZCKJ4(H29) body + ZCKE04(05) head. Please refer to the attached pictures showing the reference marked on the enclosure side, and the catalogue extract showing both functions, different. Please note that the ZCKE04 head is not sold separately; only the ZCKJ404 sub-assembly is available to order, because of the factory settings.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.