Browse FAQs

How can I prepare my Control Expert (Unity Pro) application to work with the FactoryCast features of the BMENOC0311?

Published date: 09 April 2019

Issue: How can I prepare my Control Expert (Unity Pro) application to work with the FactoryCast features of the BMENOC0311?
Product Line: Modicon M580
Environment: Control Expert (Unity Pro) v 13 or higher
Cause: N/A
Resolution:
1. In the Project browser, Right click on the Project and select Project Settings.
2. In the Project settings, under the General heading, select PLC Embedded Data.
3. Select the Checkboxes for Data Dictionary, preload on build Changes and Only HMI Variable. Click Apply.
NOTE: "Only HMI variables" does not need to be checked in order for the variables to be imported, however, it allows you to have a better control over which variables get imported to the Data Dictionary.
4. While still in the Project settings, under the General heading, select PLC Diagnostics.
5. Check the boxes for Rack Viewer Diagnostic information, Rack Viewer variable names, and Program Viewer information. Click Apply and OK.
6. Go back to your Control Expert (Unity Pro) program, open the Data Editor and select which variables you'd like to import into the Data Dictonary by clicking the HMI Variable checkbox on the desired variables.
NOTE: The BMXNOC0311 Factorycast webpages does not support all variable device types.  
7. Perform a full build on your project and transfer it into the M580 PLC.
8. In a Internet Explorer Web browser, type in the IP address of the BMENOC0311.
9. Log into the BMENOC0311 with Username: admin and Password: factorycast.
10. Navigate to the Setup Tab. Select Data Dictionary Sync from the menu on the left.
11. Press the big Start Synchronization button. The webpage will process the request for several seconds and return with "Synchronization Completed" when done.
12. Navigate to the Monitoring tab. 
13. From here, you can create a new Data Table or Chart. Under either of the Chart or Data table headings, create a new work item.
14. Select the Data Dictionary button to bring in all the variables you designated in Control Expert (Unity Pro).
15. Select variables from the populated list on the left side by clicking on them and add them to the list on the right side to be used in your new chart or table. Click OK
16. You can then view the newly created chart or table. Select the cog symbol next to the name in order to edit your work item.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.