Browse FAQs

How to set up Modbus TCP/IP Address on AccuSine PCS+

Published date: 15 March 2019

Issue
User needs to configure Modbus TCP/IP on AccuSine PCS+

Product Line
AccuSine PCS+

Environment
HMI

Resolution
To set up the Modbus TCP/IP address, perform the following steps:
  1.  Press Unit Settings
  2.  Press Display Settings
  3.  Press Advanced HMI Settings
  4.  Press the OFFLINE tab
  5.  Press Network (The HMI will shut down and restart)
  6.  Press the DHCP Tab and ensure the DHCP check box is not selected (The DHCP must be disabled to enter a Static IP)
  7.  Press Static IP
  8.  Enter the IPAddress, Subnet Mask, and Default Gateway (This will be provided by the facility's network administrator)
  9.  Press OK
  10.  Press To Run Mode
  11.  Press OK to shut down and restart the HMI

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.