Browse FAQs

Why is there a line displayed on my HMIS5T screen?

Published date: 13 November 2018

Issue:
A horizontal line or vertical line apears on the screen of an HMIS5T.


Product Line:
HMIS5T, HMISTU


Resolution:
A horizontal line or vertical line can appear on the screen of an HMIS5T when the pins of the display screen are not seated properly into the connector of the HMIS5T. Ensure that the connectors and pins are not damaged and are seated correctly. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.