Browse FAQs

How do I reset the statistical data on the Tesys-T LTMR product?

Published date: 31 October 2018

Issue:
LTMR is being moved from its original location to be used on a new application.  Customer wants to reset the statistical data on the LTMR so that they can capture accurate data in the new application.

Product Line:
LTMR Tesys-T

Environment:
All models, all serial numbers.

Cause:
Information unclear in current literature.

Resolution:
Yes.  Statistical data can be reset by pulling bit 1 of register 705 high, then returning it to a low state.   This will rest all of the statistical data registers at once.  It is not currently possible to reset statistical data registers independantly.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.