Browse FAQs

Can the M580 and BMENOC03x1 Ethernet ports auto negotiate MDIX ?

Published date: 22 October 2018


Title
M580 and BMENOC03x1 Ethernet ports auto MDIX capabilty
 
Issue
Auto MDIX feature of the M580 and BMENOC03x1 Ethernet ports 
 
Product Line
M580 BMENOC03x1
 
Environment
Unity Pro
 
Resolution
 All Ethernet ports of BMENOC0301 and the M580 CPU Ethernet ports are auto MDIX capable.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.