Browse FAQs

Osisense XC - Need XCMN2102L3 with longer cable length (8 metres)

Published date: 19 October 2018

The XCMN2102L3 is supplied with a 3m cable length, such limit switch reference exists in 5m (XCMN2102L5), 6m (XCMN2102L6), 7m (XCMN2102L7), 8m (XCMN2102L8) and 9m (XCMN2102L9). For 8m cable length, you can select the XCMN2102L8 part number. For longer lengths, please consult our Customer Care Centre

Was this helpful?

What can we do to improve the information ?