Browse FAQs

Is internet required to install / launch the Ecodial Advance Calculation?

Published date: 17 October 2018

The computer on which Ecodial Advance Calculation installed is required to be connected to the internet after the installation (only once after the installation). Once the user has completed the registration (applicable for first time user) and logged in, user can use the application without internet connection. 
If the computer on which Ecodial Advance Calculation is not connected to the internet then when user tries to launch the application for the first time, user will get a page with message "There is no internet connection" displayed. In this case, it is recommended that the user connected to the and then launches the application (for the first time user) just after the installation.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.