Browse FAQs

When monitoring LCr, Motor Current over Comms with the Process Drives, do the results vary by drive rating?

Published date: 16 October 2018

Issue:
Do the results you read for LCr, Motor Current, over Communications vary by Proces Drive Rating?

Product Line:
Altivar Process Drive

Environment:
ALL

Cause:
Wiring / Programming

Resolution:

When reading LCR unit: [A], the results are as follows
drives up to      ..D15             coeff.: 0.01
drives:     D18..  to ..C16       coeff.: 0.1 
drives higher than     C16..    coeff.: 1








Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.