Browse FAQs

Does the 170ENT11001 support the 170AMM09000?

Published date: 12 October 2018

Yes. The 170AMM09000 can be used with the 170ENT11001 adapter. It can be IO Scanned. Starting address to read from and write to is 4:1 for a length of 5.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.