Browse FAQs

What is a rating error (INF1) on an ATV320 drive?

Published date: 11 October 2018

Issue:
What is a rating error (INF1) on an ATV320 drive?

Product Line:
Altivar 320

Environment:
All

Cause:
Possible power card is different from the card stored.

Resolution:
Check the reference of the power card.
Possible internal error on drive.
Replace VFD.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.