Browse FAQs

Can motor part number BMP0702R3NA2A be used with a 230V, 3 phase input ATV320 series drive?

Published date: 10 October 2018

Issue:
Current documentation for the BMP0702R3NA2A motor shows it can be used with a single phase input ATV320 drive but does not mention the 3 phase input ATV320 series.

Product Line:
BMP0702R3NA2A motor.

Environment:
All

Cause:
Incomplete documentation.

Resolution:
Yes, the motor can be used with any 208-230 volt ATV320 series drive.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.