Browse FAQs

Osisense XC - Cross-reference of the obsolete XCKP52111 limit switch

Published date: 24 May 2019

The obsolete XCKP52111 limit switch is special switch, based on the obsolete standard XCKP521 limit switch with cable entry Pg 11, and having a head orientation different from the standard switch. Replacement by the standard XCKP2521G11 limit switch, in which the head can be turned easily

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.