Browse FAQs

How do I get the TSXCUSB485 adapter and Unitelway driver to work on a Windows XP VM?

Published date: 05 November 2018

Install the PLCUSB and Unitelway drivers are installed on both the host and VM.  Also make sure the Uniteway way is working on the Host by using the Xway test.

In the VM configuration setting the USB Controller - USB compability should be set.
User-added image
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.