Browse FAQs

Preventa XCS - How to order the XCSZC5912 part number?

Published date: 24 June 2019

Find attached the picture of both part XCSZC1 magnet and XCSZC5912 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMC5912, having a cable 2m length

Was this helpful?

What can we do to improve the information ?