Browse FAQs

Preventa XCS - How to order the XCSZP5005 and XCSZP5002 part number?

Published date: 24 June 2019

Find attached the picture of both part XCSZP1 magnet and XCSZP5005 detector which is not sold in spare parts.
Both parts are sold under complete magnetic switch XCSDMP5005, having a cable 5m length.
( XCSZP5002 has a cable of 2m length and this complete set can be ordered with the reference  XCSDMP5002 ).

Was this helpful?

What can we do to improve the information ?