Browse FAQs

Is it possible to put a keyboard infront of the IE object with Vijeo Designer V6.2?

Published date: 05 November 2018

The IE object always takes precedence on the screen over any other objects.
There is no way to put the keyboard in front of the IE object.
The solution is to make the IE object smaller or get a larger screen to fit the IE and keyboard objects.

Was this helpful?

What can we do to improve the information ?