Browse FAQs

Preventa XU - XZCP29P11L* or XZCP53P11L* pre-wired connectors M12 8-pin; material of the cable outer sheath

Published date: 28 September 2018

Material of the XZCP29P11L* or XZCP53P11L* cable outer sheath is PUR (polyurethane). It is the same for the XZCP1164L* or XZCP1264L* pre-wired connectors M12 5-pin, used for XUSL4E/2E transmitter connection


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.