Browse FAQs

Can I use the Vijeo Design'Air Plus app with a SoMachine V4.3 / Vijeo Designer V6.2 application?

Published date: 05 November 2018

The answer is No.
Only the Vijeo Design'Air is available within a SoMachine V4.3 application.

Vijeo Design'Air is just a copy of the actual HMI Target. With Vijeo Design'Air PLUS it is different. The smart phone is a second target in the HMI project.  This Android / Iphone device cannot be added as a device from SoMachine.
Vijeo Design'Air Plus is only available with a standalone version of Vijeo Designer application.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.