Browse FAQs

What can cause an ACF2 or AFE control loop fault2 on the ATV680 and ATV980 enclosed drives?

Published date: 24 September 2018

Issue:
What can cause a ACF2 or AFE control loop fault 2 on the ATV680 and ATV980 enclosed drives?

Product Line:
ATV680 and ATV980 enclosed drives

Environment:
All 

Cause:
Probable cause:
- Unstable mains voltage

Resolution:
AFE Control Loop Fault 2
Principle:
If the average value over (3ms) of the switching frequency of the AFE brick is
above 14 KHz this error occurs to protect the DC link capacitors.

Probable cause:
- Unstable mains voltage
Remedies:
- Analyze the mains voltage

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.