Browse FAQs

Can FactoryTalk be installed on a Magelis iPC?

Published date: 19 September 2018

Yes, as long as FactoryTalk supports the OS of the Magelis iPC, the software can be installed on it.

Check with the installation instructions of FactoryTalk to see if it supports the Windows OS that the Magelis iPC is running.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.