Browse FAQs

How do I know if my PC has a valid USB connection to my M221 Controller?

Published date: 05 November 2018

You can check the Device Manager.  When the USB connection is valid, the M221 Controller willl appear under the LibUsb-Win32 Devices.
If this is not active, SoMachine Basic will not connect to the M221.
This is usually the first thing to check when troubleshooting a USB connectivity issue with the M221
 

Was this helpful?

What can we do to improve the information ?