Browse FAQs

What is the maximum number of data points we can configure in IEC104 Protocol for BMXNOR0200

Published date: 18 September 2018

If our BMXNOR0200 is updated with  Firmware V1.7 IR15B, then we can have upto 7000 points configured in the configuration of BMXNOR0200 module for IEC104 protocol.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.