Browse FAQs

How can you set up PID preset setpoints on the ATV61/ATV71 drives?

Published date: 24 September 2018

Issue:
How can  you set up PID preset setpoints on the ATV61/ATV71 drives?

Product Line:
ATV61/ATV71

Environment:
All 

Cause:
PID preset set point 


Resolution:
2 preset PID ref.] [No] (nO)

nO
LI1

 [No] (nO): Function inactive
 [LI1] (LI1)

If the assigned input or bit is at 0, the function is inactive.
If the assigned input or bit is at 1, the function is active.

Set PID preset 2 speed to your 2nd setpoint for PID

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.