Browse FAQs

Does an XMIT in the Modicon Quantum Standby CPU send messages?

Published date: 12 September 2018

It is possible for an XMIT block to send messages from the Standby PLC. Use the following guidelines for Modicon Quantum Hot Standby programming with ProWORX NxT.

1. Do not place the XMIT block in the first network / section.
2. Make the XMIT run on the condition that the PLC is Primary. This will make sure that it does not trigger when in Standby mode.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.