Technical FAQs

Ask a Question

What are the minimum system requirements to install Rapsody?

Before installing the Rapsody software, make sure that below requirements are met
1. We officially tested and verified the working of Rapsody in Windows 7 and Windows 8 operating systems.
2. Admin rights should be available for the user to install and working in the software
3. Microsoft redistributable package should be available (please see the snapshot below)


4. 32 bit or 64 bit operating machines
Was this helpful?
What can we do to improve the information ?