Browse FAQs

Which Microsoft windows operating system is approved for Vijeo XL V8.0 ?

Published date: 07 September 2018

Vijeo XL is approved to work with the following operating systems
 
  • Windows 7 Service Pack 1/Professional/Enterprise/Ultimate
  • Windows 8.1 Pro/Enterprise
  • Windows 10 Home/Pro/Enterprise
  • Windows Server 2008 R2 Service Pack 1
  • Windows Server 2012 R2
  • Windows Server 2016
  • Windows Embedded Standard 7
  • Windows Embedded 8.1 Industry Pro / Enterprise
  • Windows 10 IoT Enterprise 2016 LTSB

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.