Browse FAQs

ATV320 Why don't I see drC in the Menu like I had on the ATV31 and ATV312 that I'm replacing

Published date: 16 October 2018

Issue
Why don't I see drC in the Menu like I had on the ATV31 and ATV312 that I'm replacing

 
Product Line:  
ATV320, ATV61, ATV71, Process Drives
 
Environment
All

 
Cause:
Programming


Resolution:
Simply Start  "SIn" on the ATV320, ATV61/71, and the Process Drives is the same as "drC" on ATV31/312.
You can also Press the dial [Enter] > ConF > FULL > (from here menu structure closely follows ATV312) SIn, SEt,  I_0-, CtL, FLt...

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.