Browse FAQs

When does the output of a SFC transition section gets resetted.

Published date: 05 November 2018

The transition section is executed only when the previous step is active.

When previous step is not active - even if you reset a variable before the AND block in FBD transition section the output remains to 1 because the transition action is not executed as shown in the video below
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.