Browse FAQs

What are the ION7400 Serial Communication Ports

Published date: 19 October 2018

Issue
Supported communication ports and protocols on ION7400.

Product Line
ION7400 series

Environment
Communication port/protocol.
 
Cause
Communication ports and protocols available on ION7400.

Resolution
The meter supports serial communications through its RS-485, optical and USB ports.

COM1: RS485

COM2: Optical Port (can also be configured for energy pulsing)

COM3: Micro USB (available on meters with integrated display only)

The following table illustrates what protocols are supported by each port:

          

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.