Browse FAQs

Can I convert a decimal to a hexadecimal format string with SoMahine

Published date: 04 September 2018

For example the decimal value is 2582.  The resuld would be A16 in a string.

Solution.  OSCAT Basic library from : http://store.codesys.com/oscat-basic.html
Use the DWORD_TO_STRH function block.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.