Browse FAQs

Osisense XM - XMLP025BC21F fluid conduit diameter

Published date: 07 June 2019

XMLP025BC21F fluid conduit diameter = 4mm
This data is valid for all the XMLP pressure ranges up to 60bar included. From the XMLP high pressure 100bar, a pulse snubber is integrated into fluid conduit.

Was this helpful?

What can we do to improve the information ?